Question
Output of Voltage reference buffer does not match expected value.
I set up the VREFBUF (using CubeMx) to use the internal voltage reference, with a SCALE of 2.048V. When i probe the Vref pin i see a voltage of around 2.2-2.3V, it changes slightly after ever power reset. It is a custom board with a G061c8 micro. The vref pin is not connected to any capacitors or any other pins.
I tried the same thing on a G071 nucleo board and i got exactly 2.048V on the Vref pin.
Any help is appreciated.