Question
Nucleo STM32F4012RE with StdPeriph USART Issue
Posted on November 21, 2015 at 13:26
Hi,
I've been trying to get USART working on my Nucleo board with the StdPeriph Libraries. (I haven't moved to HAL yet). Anyway, I have followed clive'1 post from [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/USART%20example%20code%20for%20Nucleo%20F401RE&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=1777]here but it does not seem to work on my Nucleo and I cannot figure out why.Here is what I've got:/* Includes ------------------------------------------------------------------*/#include ''stm32f4xx.h''#include ''stm32f4xx_gpio.h''#include ''stm32f4xx_i2c.h''#include ''stm32f4xx_usart.h''#include ''stdio.h''#ifdef __GNUC__ /* With GCC/RAISONANCE, small printf (option LD Linker->Libraries->Small printf set to 'Yes') calls __io_putchar() */ #define PUTCHAR_PROTOTYPE int __io_putchar(int ch)#else #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)#endif /* __GNUC__ */ /** * @brief Wait till USART finishes transmission */#define USART_WAIT(USARTx) do { while (!((USARTx)->SR & USART_FLAG_TXE)); } while (0)static uint8_t buf[64];/* Private function prototypes ----------------------------------*/void Delay(__IO uint32_t nCount);void GPIO_Configuration(void);void Initialise_I2C(void);void RCC_Configuration(void);void RCC_Configuration(void){ /* --------------------------- System Clocks Configuration -----------------*/ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);} /**************************************************************************************/ void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; /* Connect USART pins to AF */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2); /*-------------------------- GPIO Configuration ----------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; // PA.2 USART2_TX, PA.3 USART2_RX GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure);} /**************************************************************************************/ void USART2_Configuration(void){ USART_InitTypeDef USART_InitStructure; /* USARTx configuration ------------------------------------------------------*/ /* USARTx configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - One Stop Bit - No parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2, ENABLE);}void OutString(char *str){ /* Go through entire string */ while (*str) { /* Wait to be ready, buffer empty */ USART_WAIT(USART2); /* Send data */ USART2->DR = (uint16_t)(*str++ & 0x01FF); /* Wait to be ready, buffer empty */ USART_WAIT(USART2); }}/** * @brief Main program * @param None * @retval None */int main(void){ RCC_Configuration(); GPIO_Configuration(); USART2_Configuration(); OutString(''Hello World!''); while (1) { Delay(0x000FF); }}I can connect to COM port with no problem, but the output I am seeing is garbage: ''ððððððððððððððððððððððð''.I've tried the example UART project that comes with STM32Cube and it works on the same USART2. I've also had my oscilloscope hooked to PA_2 and PA_3 but could not see anything. Not sure if its my scope not picking anything or some settings on it are wrong.Any advice would be appreciated.Thanks