NUCLEO G431RB BOOT0 Pin and FDCAN Problem
Hi,
I've 2 Nucleo boards (Edit: Nucleo -G431RB )to communicate between FDCAN. I create a project using CUBEMX. Default FDCAN RX/TX is PA11/PA12. and I have no problem getting it work. All worked fine.
But I also need USB so I moved FDCAN Pins to PB9/PB8(BOOT0) it all collapsed. I cannot send a single frame to other end. TXFifo gets full and error occurs. (Also in loopback mode it works fine.)
I found something in documents that says nSWBOOT0 bit must be cleared, so I cleared but still no change.
Can anyone guide me here how to use propperly BOOT0 pin for FDCAN?
Best regards,
Zeki