Skip to main content
Nickname12657_O
Associate III
March 1, 2010
Question

New STM32F2xx zero-wait program execution up to 120MHz

  • March 1, 2010
  • 6 replies
  • 1321 views
Posted on March 01, 2010 at 13:44

New STM32F2xx zero-wait program execution up to 120MHz

    This topic has been closed for replies.

    6 replies

    supercoolman
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    I haven't seen any standard video processing (x264/NTSC/MPEG) on current Cortex-M3 board yet. And I just bought a STM3210E board few days ago XD

    gahelton1
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    Here is an interesting website. In particular, post #16.

    http://bbs.21ic.com/icview-159386-1-1.html

    janek2
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    Hi,

     Is there any preliminary preliminary documentation publictly available, or still being a secret?

    (As the new devices are already in preliminary sampling stage)

    The current consumption is close to that of Energy Micro EFM32 (180uA/MHz)

    sampling now.

    Jan

    BTW, interesting comparison here

    http://www.embedded.com/206801769?cid=NL_embedded

     

    4310239955_stm1_stmicro_com
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    Hi,

     Any update on the new device, yet?

    Jan

    janek2
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    Hi,

     No EEPROM (you can emulate it), but other things are already on current STM32s. You can do DMA transfer to/from GPIO - see appnote for timer triggered DMA. You can use FSMC to interface to FPGA, LCD, etc.

    Jan

    picguy2
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    Do any have EEPROM?  Even 64 bytes would be a BIG help.

    I would also like to see some kind of GPIO with DMA.  At least 8 data bits (an option for 16 or possibly 12 data bits would be nice.)  Will need h/w protocol lines.  CPU i/f can assume connected device knows if it is reading or writing.