Question
My first STM32 based circuit, is this circuit ok?
Posted on March 18, 2016 at 14:48
Hi,
This is my first time working away from Arduino.I am creating a simple CAN bus analyser using a STM32F105RBT6I have used parts of circuits from various evaluation boards.
But I am mainly concerned about the Power circuit. I want to be able to power from VIN or USB. Both are to be able to be powered at the same time.I have also seen similar circuits using a 8mhz or 25mhz so I am not sure which to use.The Image dialog on here doesn't seem to work on Safari or Chrome on Mac so please check out this post:http://electronics.stackexchange.com/questions/215097/is-this-stm32f-based-can-bus-circuit-ok #can-bus #stm32f105rbt6 #!stm32