Question
Migrating in same STM32 family with only memory size difference
Are there ANY changes needed to code moving in between STM32 chips in the same family? I.e. form one STM32L412 to another STM32L412 with just different memory (128K to 64K). I have a working project but when I program it to new chip it successfully programs and verifies, but the chip does not work. No measurable outputs. Tried on several chips. Program memory size is not an issue.