Skip to main content
colignya3
Associate
September 7, 2012
Question

MicroXplorer Request

  • September 7, 2012
  • 2 replies
  • 675 views
Posted on September 07, 2012 at 23:08

Wish-list:

1] Make the program also a standalone program for Linux, 32+64.

2] Make it able to generate code.

3] AND also able to import existing code,

so that one can adapt it easily  to a another processor in the family

[say from STM32F103 to STM32F405].

4] Fix problems when trying to use as Eclipse plug-in.

At this stage its use is very limited by the above shortcomings.

 

It can be SOOO usefull...

It is very very neat though! I cant wait.

#microxplorer-wishlist
    This topic has been closed for replies.

    2 replies

    Mark81
    Associate III
    September 10, 2012
    Posted on September 10, 2012 at 10:20

    I completely agree with you.

    But I don't know if this forum is the right place to suggest new implementation to ST's guys.

    fauvarque.daniel
    ST Employee
    September 12, 2012
    Posted on September 12, 2012 at 14:28

    Actually we try to look frequently at the forum.

    MicroXplorer should work on Linux by copying the entire MicroXplorer directory on a Linux machine and then launch it with ''java -jar MicroXplorer.jar''

    Of course today there is no official support on Linux.

    Generation of code including ways to have a customer code is currently under development. I can't give you an official delivery date yet.

    Concerning the Eclipse issue, do you have it on Windows or only on Linux ?

    Regards

    Daniel

    ​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.