Skip to main content
jelinpe7
Visitor II
February 14, 2015
Question

Meassuring frequency of external signal

  • February 14, 2015
  • 2 replies
  • 581 views
Posted on February 14, 2015 at 12:39

Hi, is it possible to meassure frequency of external signal via Input capture, if the external signal is only from 0,5V to 2,5V (not from 0V to Vdd - 3V) and it is sine wave (not square wave)?

Thank you

    This topic has been closed for replies.

    2 replies

    raptorhal2
    Lead
    February 14, 2015
    Posted on February 14, 2015 at 15:22

    Check the ''I/O Port Characteristics'' section in the data sheet for your device. For example, the F405 minimum signal voltage is 2 volts.

    Sine or square wave shouldn't matter, but the measured frequency for each sample will be more effected by signal noise for the sine wave.

    Cheers, Hal

    Tesla DeLorean
    Guru
    February 14, 2015
    Posted on February 14, 2015 at 16:18

    There is a schmitt trigger on the input, it should be able to do a reasonable job of thresholding the signal as described.

    Depending on the frequency you'd either want to count the number of pulses over a observation interval, or use the input capture to measure the period of a single cycle (or multiple using the input prescaler).
    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..