Skip to main content
EJian.1
Visitor II
February 22, 2022
Question

May I ask what is the silk screen of the material STM32F301K8U7, we are coming from F3018K7, but the specification is F3018K, which one is correct?

  • February 22, 2022
  • 1 reply
  • 675 views

..

This topic has been closed for replies.

1 reply

Peter BENSCH
Technical Moderator
February 22, 2022

Welcome, @EJian.1​, to the community!

The STM32F301K8U7 has the marking F301K87 (not F3018K7).

The marking F301K8 (not F3018K) stands for the STM32F301K8U6, i.e. the temperature range of -40...+85°C instead of -40...-105°C.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.