Skip to main content
all
Associate
February 29, 2016
Question

maximum frequency of STM32F0 @2,5v

  • February 29, 2016
  • 5 replies
  • 1325 views
Posted on February 29, 2016 at 15:57

Hi, 

What is the maximum frequency of STM32F030F4P6 at 2,5V ?

Does the supply voltage have an impact on choice of capacitor value ?

I'm planning to use 20pf capacitors and 8 mhz crystal 

On the STM32F0 discovery schematics, there is R22 resistor connected to the crystal with a value of 390ohm. Is it required ?

Thanks

#stm32f030f4p6
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
February 29, 2016
Posted on February 29, 2016 at 17:31

The capacitor and resistor values would depend on the characteristics of your chosen crystal. I would check the manufacturer's specifications, and part numbering schemes, to get a starting point there. There maximum frequency of the STM32F0 is going to be dependent on the speed of the transistors due to the CMOS process window, voltage, temperature and critical paths in the design. The flash array is likely to be a big contributor here, as it is large and slow. The 32-bit timers in the peripheral realm.

What does the data sheet indicate? There is usually a table of voltage, speed, and flash wait states. Look also at the L0 parts, these are apt to be viable at lower voltages.

The use of USB is also predicated on sufficient voltages for the pin drivers to meet specifications.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
all
allAuthor
Associate
March 1, 2016
Posted on March 01, 2016 at 12:40

Hi,

Thanks for your reply

There is no indication of other maximum operating frequency when running at lower voltage than 3V3

The datasheet only indicate operating rate from 0-48mhz and voltage 2,4-4,0 an

mcu consumption @ 3v3 

Self.Glenn
Visitor II
March 1, 2016
Posted on March 01, 2016 at 21:14

Hi,

Page 74 of document titled:

STM32F051x4 STM32F051x6 STM32F051x8

Lists maximum frequency <2.7V @20MHz

>= 2.7V is 30MHz

Glenn

all
allAuthor
Associate
March 2, 2016
Posted on March 02, 2016 at 01:00

Thanks in STM32F030 manual, there's not such limit

Anyway to be safe I will not go higher than 16 MHZ

Amel NASRI
Technical Moderator
March 2, 2016
Posted on March 02, 2016 at 15:31

Hi gfranck,

As general recommendation: besides to referring to the operating conditions stated in 

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00088500.pdf

, I suggest you have a look to the 

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00089834.pdf

 (Getting started with STM32F030xx hardware development). This later provides tips on how to set your hardware in order to use STM32F030x devices in adequate conditions.

-Mayla

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.