Skip to main content
idrissmc
Associate III
July 17, 2019
Question

Localisation of program in Flash memory

  • July 17, 2019
  • 0 replies
  • 448 views

Hi everyone,

I wonder how to know from which address start a program when we debug it into the flash memory and the finish address is easy to find if we know the start address.

according to the map of flash memory of the STM32F413 given by the link below:

https://www.st.com/content/ccc/resource/technical/document/reference_manual/group0/81/ea/88/1f/97/9e/4a/d0/DM00305666/files/DM00305666.pdf/jcr:content/translations/en.DM00305666.pdf

On page 67: we see that there are some place which are reserved, I wonder if these place are reserved for the program through the ST-link?

or maybe if the program is more large then we will exceed these limits?

can someone cleared to me this point?

thank you

This topic has been closed for replies.