Is anyone done USART in STM32L4R9I-DISCO Discovery Kit please share ... I have trouble doing LPUSART
UART_HandleTypeDef hlpuart1;
///init///
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = 256000;
hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart1.Init.StopBits = UART_STOPBITS_1;
hlpuart1.Init.Parity = UART_PARITY_NONE;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
hlpuart1.FifoMode = UART_FIFOMODE_DISABLE;
uint8_t Test[] = "Hello World !!!\r\n"; //Data to send
if (HAL_UART_Transmit(&hlpuart1,Test,sizeof(Test),100)!= HAL_OK)
{
Error_Handler();
}