Is it OK to enable internal pull up on port pin that could be exposed to 5 volts? The pin is a five volt tolerant pin. I presume the internal pull resistor is connected to VDD (3v3 in my case) therefore there would be a small current flowing from the port pin (5V) through the internal pull up to 3v3. It works but I was just wondering if it might damage the processor in time. Regards Trevor