Skip to main content
progettazione
Visitor II
May 26, 2016
Question

Input impedance on SDADC pin of STM32F373

  • May 26, 2016
  • 0 replies
  • 515 views
Posted on May 26, 2016 at 16:00

Hi, eveybody.

I read that the input impedance on a SDADC input should be from 47k to 640k (more or less) and depends on gain and clock frequency.

Let's suppose that a 100k ohm impedance is needed.

Can the input impedance of a SDADC input be like the one in the image?

0690X000006038qQAA.jpg

MIS_Iout is the signal for the SDADC input.

I_OUT is a 0-5V signal that I need to reduce to the 0-3.3V range (because the Vref for the SDADC is 3.3V).

Regards

Igor
    This topic has been closed for replies.