Skip to main content
Luis Ber
Associate II
September 23, 2019
Question

Incorrect Get Time from RTC (year 2035 for example)

  • September 23, 2019
  • 0 replies
  • 456 views

Hello everyone,

I have an application that synchronizes the RTC with the current time using a 3G module. Once it is synchronized, the system gets the date and time every 5 minutes in order to store sensor samples with a real timestamp. Everything is fine, but sometimes the value that I get using Get_Time from the RTC is incorrect (the year is 2035 for example).

It's very difficult to repeat the error and I cannot see where is the problem. Do you think that it could be a hardware problem (due to the possible noise produced by the 3G module affecting LSE crystal)? What other thing could produce these type of problems?

I'm using a STM32L451VCT6. And the initialization code is the following:

memset(&mainApp.newDateTime, 0, sizeof(Synchronization_DateTime_t));
 
mainApp.newDateTime.time_date.Year = MAINAPP_DEFAULT_DATE_YEAR;
mainApp.newDateTime.time_date.Month = MAINAPP_DEFAULT_DATE_MONTH;
mainApp.newDateTime.time_date.Date = MAINAPP_DEFAULT_DATE_DAY;
mainApp.newDateTime.time_date.WeekDay = RTC_WEEKDAY_MONDAY;
 
mainApp.newDateTime.time_time.Hours = MAINAPP_DEFAULT_HOUR_HOURS;	mainApp.newDateTime.time_time.Minutes = MAINAPP_DEFAULT_HOUR_MINUTES;
mainApp.newDateTime.time_time.Seconds = MAINAPP_DEFAULT_HOUR_SECONDS;
mainApp.newDateTime.time_time.SubSeconds = MAINAPP_DEFAULT_HOUR_SUBSECONDS;
 
HAL_RTC_SetTime(timeManager.phrtc, &pNewDateTime->time_time, FORMAT_BIN );
HAL_RTC_SetDate(timeManager.phrtc, &pNewDateTime->time_date, FORMAT_BIN );

Any help will be appreciated.

Thank you very much.

Luis

This topic has been closed for replies.