Skip to main content
russell2
Visitor II
July 18, 2014
Question

IMAGE_SetPNG is not defined in STemWin library

  • July 18, 2014
  • 1 reply
  • 638 views
Posted on July 18, 2014 at 21:18

Hi,

I'm getting the following build error, it appears ''IMAGE_SetPNG'' is not defined in STemWin library.

Building configuration: Project - STM324x9I_EVAL_MB1046

Updating build tree...

kohler_windowDLG.c 

Linking

Error[Li005]: no definition for ''IMAGE_SetPNG'' [referenced from C:\Users\kocd3y3\Downloads\ST\stm32cubef4\STM32Cube_FW_F4_V1.3.0\Projects\STM324x9I_EVAL\

Applications\STemWin\STemWin_SampleDemo\EWARM\STM324x9I_EVAL_MB1046\Obj\kohler_windowDLG.o]

Error while running Linker

 

Total number of errors: 1

Total number of warnings: 0

    This topic has been closed for replies.

    1 reply

    Montassar BEN ROMDHANE_O
    Visitor II
    August 6, 2014
    Posted on August 06, 2014 at 13:53

    Higrensing.russell.001,

    Please ensure that kohler_windowDLG.c file is including the dialog.h header file which includes also the IMAGE.h header file containing the IMAGE_SetPNG() STemWin function prototype:

    void IMAGE_SetPNG (IMAGE_Handle hObj, const void * pData, U32 FileSize);

    Thank you for your interest in our STM32Cube solution. With regards.