Question
I2C interrupt mode only works once?
Posted on June 21, 2016 at 14:53
I follow the example of the I2C_TwoBoards_ComIT
I have I2C host to send data to the STM32L4 board. The I2C slave has below logic HAL_I2C_Slave_Receive_IT(&I2cHandle, (uint8_t *)aRxBuffer, RXBUFFERSIZE); In the HAL_I2C_SlaveRxCpltCallback, I set a flag to allow main loop to process the data. But it only works once, and the second time, it cannot receive data and cannot trigger the interrupt. May I know any other setting need to make I2C slave recieve multiple time? thanks #i2c-interrupts-stm32