I can not configure ''CubeMX SDIO DMA FatFS configuration''
Hello!
I use the microcontroller STM32F205ret6, STMCubeMX v4.22.0, Firmware vSTM32Cube_FW_F2_v1.6.0. Configured to work with SD card in SDIO + FatFs mode without DMA. Recording to the card comes at a speed of 2.5 MB / s- it suits me perfectly. I write blocks of 25600 bytes, 1 block records 15 mSec. I need to save the processor from the work of transferring data to the SD card. For this example:https://community.st.com/servlet/JiveServlet/download/1546-1-8967/SDIO+DMA+FatFS+CubeMX.pdf
&https://community.st.com/s/contentdocument/0690X0000060Hm6QAE
When unpacking an archive, you can not read its contents.
tuned SDIO + DMA. Here are my settings:
hdma_sdio.Instance = DMA2_Stream6;
hdma_sdio.Init.Channel = DMA_CHANNEL_4; hdma_sdio.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_sdio.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sdio.Init.MemInc = DMA_MINC_ENABLE; hdma_sdio.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_sdio.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_sdio.Init.Mode = DMA_PFCTRL; hdma_sdio.Init.Priority = DMA_PRIORITY_LOW; hdma_sdio.Init.FIFOMode = DMA_FIFOMODE_ENABLE; hdma_sdio.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hdma_sdio.Init.MemBurst = DMA_MBURST_INC4; hdma_sdio.Init.PeriphBurst = DMA_PBURST_INC4;main.c:
&sharppragma pack(4)
FATFS SDFatFs; &sharppragma pack(4) FIL MyFile; &sharppragma pack(4) uint8_t capture_buf[25600];Interrupts fulfills:
void SDIO_IRQHandler(void)
{HAL_SD_IRQHandler(&hsd);
}
void DMA2_Stream3_IRQHandler(void)
{HAL_DMA_IRQHandler(&hdma_sdio);
}
After exiting from HAL_SD_ReadBlocks_DMA.
Goes in cycles in anticipation: while ((HAL_SD_STATE_BUSY == state_return) && (SD_WAIT_TIMEOUT > timeout))
After the timeout, it goes out with an error.
Where is my mistake? Or is it not me?null