Question
I am using an NUCLEO-F429Zi to read a sensor over I2C. The application works correct. When the ST-Link is removed (cut away) from the board, the I2C connectivity fails. Any idea how to prevent this?
I am using an NUCLEO-F429Zi to read a MPU over I2C ( 2C1, PB8, PB9). The applications works correct. The sensor returns the correct values. When the ST-Link is removed (cut away) from the board, the power supply Vin , the I2C connectivity fails. It is still possible to program the board and to set and toggle the I2C pins (PB(, PB9).