Skip to main content
BBick.1
Associate II
October 10, 2020
Question

How to use Oversampling with H753 ADC..

  • October 10, 2020
  • 2 replies
  • 770 views

I've been trying to get Oversampling working using polling for ADC completion, but I'm not seeing the expected results. I found one example for x4 oversampling, but in reality that doesn't seem to actually be doing anything. I am trying to use 32 for the ratio using the appropriate definition from the include file. But when I do that I wind up with a value that is about one fourth what it should be. So I'm looking for a working example of oversampling with this processor.

Thanks,

This topic has been closed for replies.

2 replies

TDK
Super User
October 13, 2020
BBick.1
BBick.1Author
Associate II
October 13, 2020

Thanks for the pointer to the example. When I attempted to use the oversampling configuration I was not getting correct results. Digging into the specs for the 753 MCU we are using I was able to resolve the issue and now get consistent results, and within the expected tolerance for the voltage that is being monitored.