Question
How to select a particular peripheral for a pin on F107
Posted on September 05, 2016 at 19:46
Folks,
Can't see anything in the user manual about this. With the Atmel M3/M4s if you have a pin that has multiple uses such as UART/Timer/Ethernet there's a register to program that selects which of the peripherals will be routed to the pin. On the STM32 I can see no such register. So, for example, on the F107, PB10 can be I2C, USART3 or Ethernet. How does one choose the appropriate function please? Thanks! Rob