Skip to main content
phenom
Associate III
May 10, 2019
Question

How to generate PWM pulse with varying timer period?

  • May 10, 2019
  • 1 reply
  • 623 views

Hi,

I am working on STM32F56G eval board. I need to generate a PWM pulse with varying time period on a single channel. I am new to stm32 PWM. With DMA burst code example time period is changing on the runtime .

How can I generate a PWM pulse with different time period on a single channel?

Eg : 1 pulse (x time period) + 2 pulse (y time period) +3 pulse (x time period)

If it is possible to generate such PWM pulse pattern then please suggest approach or example code.

Any help is appreciated.

This topic has been closed for replies.

1 reply

S.Ma
Principal
May 10, 2019

Chose a timer with DMA channel on the channel, and define a marco period of 6 pulse period.

Use the DMA cyclic table to go through the 12 toggle events.

Is this what you need implemented?

phenom
phenomAuthor
Associate III
May 13, 2019

Thanks.

I want to implement a pattern of pulse with varying time periods.

A output on oscilloscope should be like :

A pulse (1Khz) + delay (200ms) + pulse (2KHz) +..

Where I need to add delays between pulses.

Any steps to achieve such a pattern is helpful.