Skip to main content
ludovic-micou2
Associate II
January 13, 2022
Question

Hello, I have a short circuit between the RESET and the VCC. I measure a impedance of 1ohm between these two signals and 80ohm with the GND. The RESET pin only goes on a 0.1UF capacitor and on the programming connector.

  • January 13, 2022
  • 2 replies
  • 1527 views

the ST-LINK can't detect the micro but the software who is already programmed in the micro work perfectly.

Does anyone have an explanation why the reset breaks like this?

    This topic has been closed for replies.

    2 replies

    TDK
    January 13, 2022

    If NRST is shorted to VCC, there's a hardware error or you've damaged the chip. There's no setting you can enable that would do this.

    Likewise, if VCC has 80 Ohm impedance to ground, that also indicates a likely hardware error.

    Also possible you're measuring it incorrectly, such as with the debugger attached or with it powered.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    lmico.1
    Visitor II
    January 13, 2022

    The measurement was made with the power and probe cables disconnected from the board. The measurement