Hello I am trying to establish single-byte receive on stm32f091 controller by polling mode but unable to do it . Do i need to monitor any flag or clear any of the flag. Please suggest some solution.
uint8_t tx_Data[4]="AT\r\n";
uint8_t tx_Data_A[26]="ATFY0K0C0R0S30=64S0=0@L1\r\n";
uint8_t tx_Data_B[5]="ATD\r\n";
uint8_t rx_Modem0[40];
uint8_t rx_Modem1[40];
HAL_UART_Transmit(&huart1, tx_Data, 4, 400);
//HAL_Delay(500);
HAL_UART_Receive(&huart1,rx_Modem0, 40, 2000);
HAL_UART_Transmit(&huart1, tx_Data_A, 26, 400);
//HAL_Delay(500);
HAL_UART_Receive(&huart1,rx_Modem0, 40, 2000);
HAL_UART_Transmit(&huart1, tx_Data_B,5, 10);
//HAL_Delay(500);
HAL_UART_Receive(&huart1,rx_Modem0, 40, 1000);