Hard fault thrown in NVIC_Init !
Hi,
I am using the STM32L151VC mpu and I have run into a problem in that a hard fault is being thrown by a seemingly innocuous bit of code inside the STM32L1xx_StdPeriph_Lib_V1.1 in the NVIC_Init() function. The line is line 146 from the file STM32L1xx_StdPeriph_Driver\src\misc.cas follows :
/* Compute the Corresponding IRQ Priority --------------------------------*/
tmppriority = (0x700 - ((SCB->AIRCR) & (uint32_t)0x700))>> 0x08; The hard fault is thrown by the central part of this which I have extracted out as follows :
/* Compute the Corresponding IRQ Priority --------------------------------*/
// tmppriority = (0x700 - ((SCB->AIRCR) & (uint32_t)0x700))>> 0x08;
uint32_t *** = (SCB->AIRCR) & (uint32_t)0x700; // !!!!!!! Problem
tmppriority = (0x700 - ***)>> 0x08; I have checked the disassembled line which seems completely innocuous :
ldr r3, [r3, #12]r3 has the value 0xe000ed00 at the start of the instruction which agrees with the values for SCB->AIRCR from core_cm3.h. SCB is defined as 0xE000E000UL + 0x0D00UL, and AIRCR is the 4th uint32_t (ie offset 0x0C) defined in SCB_Type, also in core_cm3.h.
The output from the hard fault handler I am using is :
Hard fault handler - all numbers in hex :
R0 = 20001df4 R1 = 40013800 R2 = 40013800 R3 = e000ed00 R12 = 8001a95 LR [R14] = 8000b33 subroutine call return address PC [R15] = 8000d7e program counter PSR = 21000000 Bus Fault Address Reg, BFAR = e000ed0c Configurable Fault Status Reg, CFSR = 8200 Hard Fault Status Reg, HFSR = 40000000 Debug Fault Status Reg, DFSR = 1 Auxiliary Fault Status Reg, AFSR = 0 Sys Hdlr, Ctrl & State Reg, SCB_SHCSR = 0I assume I must be doing something wrong but can't see for the life of me what it is, any ideas greatefully received.
Thanks,
Mike