Skip to main content
baranovus
Associate III
January 26, 2016
Question

HAL based ADC-DMA makes only one transaction

  • January 26, 2016
  • 1 reply
  • 503 views
Posted on January 26, 2016 at 20:03

Hello. I try to make a simple non-continuous ADC-DMA transaction of 10 measurements. I get only one sample in my array. I don't use interrupts, just wait for DMA completion. Could you tell, what I am doing wrong?

Here are my functions (I am sorry if there exist some codebox tag and I did not notice it):

UINT16 Adc1ShortReadBuf[10];

void Get10Samples(void)

{

DMA_HandleTypeDef DmaHandle1;

DmaHandle1.Init.Channel = DMA_CHANNEL_0;

DmaHandle1.Instance = DMA2_Stream4;

HAL_DMA_DeInit(&DmaHandle1);

DmaHandle1.Init.Direction = DMA_PERIPH_TO_MEMORY;

DmaHandle1.Init.PeriphInc = DMA_PINC_DISABLE;

DmaHandle1.Init.MemInc = DMA_MINC_ENABLE;

DmaHandle1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;

DmaHandle1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;

DmaHandle1.Init.Mode = DMA_NORMAL;

DmaHandle1.Init.Priority = DMA_PRIORITY_HIGH;

DmaHandle1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

DmaHandle1.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_HALFFULL;

DmaHandle1.Init.MemBurst = DMA_MBURST_SINGLE;

DmaHandle1.Init.PeriphBurst = DMA_PBURST_SINGLE;

HAL_DMA_Init(&DmaHandle1);

ADC_ChannelConfTypeDef sConfig;

sConfig.SamplingTime = ADC_SAMPLETIME_112CYCLES;

sConfig.Rank = 1;

sConfig.Offset = 0;

ADC_HandleTypeDef AdcHandle1;

ADC_MultiModeTypeDef multimode;

AdcHandle1.Instance = ADC1;

HAL_ADC_DeInit(&AdcHandle1);

AdcHandle1.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV8 ;

AdcHandle1.Init.Resolution = ADC_RESOLUTION12b;

AdcHandle1.Init.ScanConvMode = DISABLE;

AdcHandle1.Init.ContinuousConvMode = DISABLE;

AdcHandle1.Init.DiscontinuousConvMode = DISABLE;

AdcHandle1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

AdcHandle1.Init.ExternalTrigConv = ADC_SOFTWARE_START;

AdcHandle1.Init.DataAlign = ADC_DATAALIGN_RIGHT;

AdcHandle2.Init.NbrOfDiscConversion = 0;

AdcHandle1.Init.NbrOfConversion = 1;

AdcHandle1.Init.DMAContinuousRequests = DISABLE;

AdcHandle1.Init.EOCSelection = DISABLE;

HAL_ADC_Init(&AdcHandle1);

multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES;

multimode.Mode = ADC_MODE_INDEPENDENT;

multimode.DMAAccessMode = ADC_DMAACCESSMODE_DISABLED;

HAL_ADCEx_MultiModeConfigChannel(&AdcHandle1, &multimode);

DMA_ClearTCFlag(&DmaHandle1);

sConfig.Channel = ADC_CHANNEL_0;

HAL_ADC_ConfigChannel(&AdcHandle1, &sConfig);

__HAL_LINKDMA(&AdcHandle1, DMA_Handle, DmaHandle1);

ADC_DMA_start(&AdcHandle1, (uint32_t*)Adc1ShortReadBuf, 10);

}

HAL_StatusTypeDef ADC_DMA_start(ADC_HandleTypeDef* hadc, uint32_t* pData, uint32_t Length)

{

__IO uint32_t counter = 0;

/* Enable ADC DMA mode */

hadc->Instance->CR2 |= ADC_CR2_DMA;

/* Set src and dst addresses and length*/

HAL_DMA_Start(hadc->DMA_Handle, (uint32_t)&hadc->Instance->DR, (uint32_t)pData, Length);

/* Check if ADC peripheral is disabled in order to enable it and wait during

Tstab time the ADC's stabilization */

if((hadc->Instance->CR2 & ADC_CR2_ADON) != ADC_CR2_ADON)

{

/* Enable the Peripheral */

__HAL_ADC_ENABLE(hadc);

/* Delay for ADC stabilization time */

/* Compute number of CPU cycles to wait for */

counter = (ADC_STAB_DELAY_US * (SystemCoreClock / 1000000));

while(counter != 0)

{

counter--;

}

}

hadc->Instance->CR2 |= ADC_CR2_SWSTART;

/* Return function status */

return HAL_OK;

}

Solved it. Conversion has to be continuous. Actually, the post can be deleted.

AB

    This topic has been closed for replies.

    1 reply

    Amel NASRI
    Technical Moderator
    January 28, 2016
    Posted on January 28, 2016 at 11:14

    Hi baranov.aleksandr,

    I don't agree to delete the post.

    It should be kept to help other users that may face same issue.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.