Skip to main content
jveith
Associate II
June 8, 2011
Question

H-Bridge circuit for Advanced Timer using a DC brush motor

  • June 8, 2011
  • 0 replies
  • 484 views
Posted on June 08, 2011 at 16:23

anybody knows a application note for a circuit with 4 N-channel mosfets or 2 P/N channel pairs. My DC brush motor is about 24V 6 Amp and I prefere to use the complementary outputs for Timer 1 / Timer 8 with programmable deadtime instead of integrated H-Bridge

    This topic has been closed for replies.