Question
GPIO on STM32479I-EVAL evaluation board
Posted on September 14, 2016 at 20:49
Hello,
We have a need for over 32 GPIO's in our system for both GPIO and Clocking signals.We also need access to the the I2C ports - I2C0 and I2C2?Has anyone analyzed and produced a Pin-Mux matrix of the GPIO's on the STM32479I-EVAL evaluation board(other than the tables in the User Manual) to determine access of the GPIO's other than the MFX eXpander connector? Such as the CN5 - CN6 and C10 - C11 connectors?Questions:We wanted access to:1. Another I2C port such as I2C0 and I2C 2?2. Are the signals on C10 and C11 ONLY for Memory interfaces or can we use this pins for GPIO?Thank you.JT #stm324 #stm32 #gpio #stm32eval