Skip to main content
dmilovanovic9
Visitor II
September 10, 2015
Question

Get the stack size during application

  • September 10, 2015
  • 5 replies
  • 2175 views
Posted on September 10, 2015 at 22:15

Hai, im developming an application using the ST standard peripherie library. Im trying to get the information, how big is my stack. I tried to use the __get_PSP(void) function to get the value of the stack program counter. This function is implemented into the file: core_cmFunc.h

When im executing my code, i will not get the right values. When im debuging, i can see the value in SP Register and thus the stack pointer.

Could somebody help me how to get the information, how big is my stack during my application.
    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    September 10, 2015
    Posted on September 10, 2015 at 22:57

    Define a local/auto variable which is volatile, and get the address of it.

    {

      volatile int i;

      printf(''%p\n'',&i);

    }

    or return it as a (void *) pointer

    void * getsp(void)

    {

      volatile int i;

      return(&i);

    }

    The more classic way of measuring stack depth and utilization, is to clear or mark the entire stack space, and then periodically go the the base address for the stack section (not the SP at the top), and move upward until you no longer see you initialization pattern.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    waclawek.jan
    Super User
    September 10, 2015
    Posted on September 10, 2015 at 23:01

    Stack pointer is R13; how to get its value is compiler-dependent.

    The value of information obtained in this way is dubious; the 0xDEADBEEF watermark method (google for it if you don't know it already) might be more adequate.

    JW

    jpeacock
    Associate
    September 11, 2015
    Posted on September 11, 2015 at 14:00

    If you are using interrupts you can periodically check stack pointers (process and system) to look for highwater marks (i.e. lowest address).  Not all that reliable but easy and sometimes it gives you an early warning when a stack exceeds it's bounds.

    FreeRTOS uses a variation on this.  When task context changes there's an option to check task stack pointer to ensure it's in range.  Saved me some debugging on several occasions.  You still need to do your own checks for system SP, especially if nesting interrupts.

      Jack Peacock

    LMI2
    Senior III
    September 11, 2015
    Posted on September 11, 2015 at 19:34

    Interesting.

    How do you get R13 value? Or how do you easily mix assembly and C?

    For example in Keil 5?

    Tesla DeLorean
    Guru
    September 12, 2015
    Posted on September 12, 2015 at 02:07

    Surely something like this is significantly more portable, although implementation dependent.

    int main(void)
    {
    volatile void *x = &x;
    ...

    volatile should prevent it optimizing to a register, as should getting it's address. ie forces it to be memory, as registers don't have and address. If you want to learn how to inline assembler with __asm I'm sure there's documentation, but ARM/Keil does make it difficult to access R.R15
    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..