Skip to main content
hassan23
Visitor II
April 22, 2016
Question

Flash program error when using fast mode

  • April 22, 2016
  • 0 replies
  • 514 views
Posted on April 22, 2016 at 19:09

Hi, 

   I am trying to use the fast program method to write a row (256 bytes) to the flash. But when HAL_Flash_Program() function is called, the PGAERR flag is raised. The input buffer as well as the write address are 256 byte aligned.

#flash #stm32l476
This topic has been closed for replies.