Skip to main content
jaeshik
Visitor II
January 17, 2016
Question

flash memory endurance of STM32F030

  • January 17, 2016
  • 1 reply
  • 687 views
Posted on January 17, 2016 at 03:08

Hi~

I'm under review for EEPROM emulation on STM32F030.

but, I found that flash memory endurance is min 1000 cycle(1K).

Unfortunately, It is short to use in my project.

Do you know why it is shorter than other STM32?

Most of the other STM32 is a flash endurance is min 10K.
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    January 17, 2016
    Posted on January 17, 2016 at 15:41

    Based on the design, process geometry and testing, they have less confidence in the long term performance?

    If you really need EEPROM, use one instead of pretending that FLASH is a substitute. Consider if NVRAM is an alternative.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..