Question
First step with Nucleo F091RC
Posted on April 21, 2015 at 10:35
Hello everybody,
I got a Nucleo F091RC and I'm starting programming but it is pretty complex. I use Coocox and GCC compiler. I try to understand how my board works with the HAL libraries. First I would like to change the clock system in the ''system_stm32f0xx.c'' (which is 8MHz) and I'd like to work at 48MHz using HSE and PLL MULL * 6. Then I'd like to know how to configure the different peripheral structures : eg. RCC_OscInitTypeDef / SPI_HandleTypeDef / UART_HandleTypeDef / etc... I try to find where these structures are declared and what parameters I can put into them but I only found example, not showing exactly my expectations... Thank you all for your help to a beginner :)