Failed to read ROM table via AP 3
- August 31, 2023
- 1 reply
- 2954 views
Hi to everyone, I'm looking for help regarding a problem to start a dual core project debugging.
In order to make things as much clear as possible I've decided to start a new project by selecting the "DualCore_Standalone" example related to the STM32H747I-EVAL board (I'm working with the STM32H757I-EVAL).
Starting from this example I've configured the CM7 and CM4 debugger, according to the AN5361.
At this point when I start the debugging session on the CM4 (after starting the CM7 debugging session), I get the following error:
STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\Asus\STM32CubeIDE\workspace_1.10.1\DualCore_Standalone\STM32CubeIDE\CM4\Debug\CM4_st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61238
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
COM frequency = 24000 kHz
Target connection mode: Attach
Failed to read ROM table via AP 3
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
More over in the attached files can be found the debugger log related to both cores.
Any clue?
Thanks in advantage for the help,
Luca.
PS:
Some other useful information:
STM32CubeIDE, Version: 1.13.1, Build: 17479_20230728_0839 (UTC)
STMicroelectronics ST-LINK GDB server. Version 7.4.0