Question
F373 current in Stop Mode too large
Posted on April 19, 2013 at 16:49
VDDC should be 5uA, AVDD should be 2uA. But I have 500uA. I tried to enter in the stop mode before and immediately after the system_init, without any initialization settings. Tried also to do pins IN, FLOAT, AF. Stop and Standby. WFI and WFE. Trying to run the RTC, and without it - the result is the same >500uA. Where the deuce? By the way, with L15x had no such problems.