Skip to main content
Myasu.1
Associate III
August 13, 2021
Question

Error finishing flash operation

  • August 13, 2021
  • 1 reply
  • 1292 views

I have the following error when I was trying to debug using TrueStudio(v9.3.0).

0693W00000D2PylQAF.pngThe specific steps that caused the error are as follows.

1. Connect STM32F100RB※1 to the PC.

2. Launch TrueStudio(v9.3.0)

3. make project

3.1 [File] -> [New] -> [C Projet]

3.2 Select Embedded C Project

3.3 Select [STM32F1] -> [STM32VL_Discovery]

3.4 Next (default setting)

3.5 Next (default setting ※2)

3.6 finish

4. debug project

4.1 [Run] -> [debug configuration]

4.2 Select [EmbeddedC/C++ Application]

4.3 Push [debug] bottun

4.3 the above error is output

※1 STM32VLDISCOVERY - Discovery kit with STM32F100RB MCU - STMicroelectronics

※2 ST-LINK is selected​

Could you please confirm?​

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    August 17, 2021

    Hello @Myasu.1​ and welcome to the Community :)

    Have you tried with old release of TrueStudio (uninstall v9.3.0 TrueStudio version and install for example Version 9.0) ?

    Please keep me informed about your update.

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks