Doubt about interrupt priority
Hi, I have a doubt about interrupt priority.
Let's say we have two ISRs for two interrupts: interrupt A and interrupt B, where A has a higher priority than B.
If the ISR of B is running and an interrupt A arrives, then the ISR B is interrupted, that of A is executed, and then the ISR of B is resumed.
But if the ISR of A, the interrupt with the highest priority, is running and an interrupt B arrives, what happens? Is interrupt B ignored and continuing to execute ISR of A, or the B ISR is queued and executed after A ISR and then continuing with the normal program?