Skip to main content
ARam .1
Visitor II
April 9, 2020
Question

Does stm32f767zi support 3 CANs as slave?

  • April 9, 2020
  • 1 reply
  • 555 views

in STMCubeMX it says that CAN1 and CAN3 are master and CAN2 is slave. I need to use all three CANs as slave.Would it be possible to do that? If i can do that would i just be configuring the CAN1 and CAN3 as master in STMCubeMX and continue to use them as slaves?

This topic has been closed for replies.

1 reply

Bowman32
ST Employee
April 14, 2020

Hello @ARam .1​ 

Yes you can use CAN1 and CAN3 as master and continue to us them independently.

Best regards,

Bouraoui