Question
DMA transfer (Reception) not proper when implemented with ethernet communication
Posted on November 24, 2014 at 07:54
Hello there,
I am using Lwip library for Ethernet implementation. I poll for the Ethernet packet in main loop. Then the packet is passed to further libraries to process it. Meanwhile I have also to receive 8 bit data on Port GPIOH with clock on Timer 8 capture. Using DMA2, channel 7. Receiving 220 bytes of parallel data @20 Mhz. DMA transfers it from GPIO port H to internal RAMIf I run the DMA without ethernet, it runs perfectly fine. but when ethernet is switched on, some of the DMA packets are lost.Did a test and found 400 packets out of 100000. (0.4%)Do not have sufficient window to retransmit the packet. But cannot afford to loose the packet.Hardware issues like noise etc are ruled out. Please Help.Thanks in advance #stm32f4 #dma