Skip to main content
S Syndikate
Associate
June 5, 2017
Question

Development board needed

  • June 5, 2017
  • 3 replies
  • 2958 views
Posted on June 05, 2017 at 09:46

Need a development board for STM32L4A6xG I couldnt find it folks do help me out!

    This topic has been closed for replies.

    3 replies

    Danish1
    Lead III
    June 5, 2017
    Posted on June 05, 2017 at 14:09

    There are too many different microcontrollers for someone to make a development board with each and every one.

    One approach is to buy a demo board with a similar processor such as nucleo-L476RG and ask a local surface-mount manufacturer / reworker to change the microcontroller to your preferred one.

    I note that my main component supplier (farnell UK) does not (yet) stock that microcontroller so it might be too new to even go that route yet.

    Another approach is to buy a demo board with a microcontroller that has all the features you need, even if it is in a bigger package. Farnell stock Nucleo-L496ZG. I don't think that has the crypto/AES stuff.

    Hope this helps,

    Danish

    S Syndikate
    Associate
    June 5, 2017
    Posted on June 05, 2017 at 23:44

    Thanks a lot Danish Ali, i have never thought about reworking with a

    development board, thanks a lot for that but the problem is I do not have

    any local surface mounters, thanks a bunch for the other suggestion but i

    would require a CryptoEngine for sure. And could you please correct my

    thinking if i am wrong, I think that inorder to implement a AES encryption

    on binary input and also Elliptical Curve Deffie Hellman functions i need a

    cryptoengine to make the processing time quicker, i have just implemented a

    AES encryption on an Arduino UNO and it worked, perfectly. The processing

    time was in single digit milli seconds. So what would you suggest.

    On Mon, Jun 5, 2017 at 5:40 PM, Danish Ali <st-microelectronics@jiveon.com>

    Zt Liu
    Senior III
    June 6, 2017
    Posted on June 06, 2017 at 16:39

    In the following page, 

    http://www.st.com/en/microcontrollers/stm32l4a6rg.html

    Click evaluation tools.

    You will  see so many dev kits, is that what you want?

    0690X00000602T4QAI.bmp

    Hope that helps! 

    :)

    S Syndikate
    Associate
    June 6, 2017
    Posted on June 06, 2017 at 16:42

    Yes i have found it thank you Mr.Zhitai Liu

    Where can we connect to have a personal conversation, i did find you in FB

    Samuel Schalkwyk
    Associate
    June 8, 2017
    Posted on June 08, 2017 at 10:18

    Hi

    I think you can also look at this development kit, you can get add on controller plug in modules on which you can add the chip you would need, also it has a full IDE, 

    https://www.mikroe.com/stm32/

    Regards

    Sam