Skip to main content
Cedric Boudinet
Associate III
January 21, 2022
Question

Delay generator based on STM32F429

  • January 21, 2022
  • 6 replies
  • 2394 views

Hello

I am trying to delay a 1Hz digital signal.

I would like to generate a delay varying from a few microseconds to 10 ms.

I tried to use ETR, TI1_ED and PWM input but I didn't manage to found out how to do.

Does anyone has an idea on how to proceed?

Bests

This topic has been closed for replies.

6 replies

waclawek.jan
Super User
January 22, 2022

There is no hardware to do it without software.

Set up input capture on one channel, and enable interrupt from it. That will be the input.

As output, set up other channel to compare output - don't need to set a particular mode in TIMx_CCMR.OCxM yet, just set up the pin for AF/TIMx_CHx, and enable that channel in TIMx_CCER.

Enable timer's counter by setting TIMx_CR1.CEN. Leave it at internal clock; if needed, set prescaler so that at maximum ARR it won't overflow sooner than the maximum required delay.

Then, in the capture interrupt, read out the captured value from TIMx_CCRx, add the required delay, store to the output channel's TIMx_CCRx, read the current input pin's level and set the output's mode in TIMx_CCMR.OCxM to appropriate "set to active/inactive on match".

That's all.

JW

waclawek.jan
Super User
January 22, 2022

On second thought, there may be a purely hardware solution:

  • use CH1, CH2 or ETR as input
  • select this as input to slave-mode controller, in TIMx_SMCR.TS
  • set Trigger mode in TIMx_SMCR.SMS
  • set a different channel to Output compare, set it to Toggle mode in TIMx_CCMR.OCxM, enable in TIMx_CCER
  • set appropriate polarity in TIMx_CCER (see comment below)
  • set prescaler appropriately, to avoid overflow at longest delay
  • set both TIMx_ARR and TIMx_CCRx for the output channel to value corresponding to the delay
  • set One-Pulse Mode by setting TIMx_CR1.OPM
  • enable timer by setting TIMx_CR1.CEN

The risk associated with this method is incorrect output polarity/inversion, so I'd set up an interrupt upon the first capture, and perform the whole setup including checking/adjusting polarity there.

JW

MM..1
Chief III
January 22, 2022

You dont detail how bit width is your digital signal, in teory you can delay for example 8 or 16 bit bus too.

And too if only one bit signal you can use EXTI interrupt as input(s) read event

, then timer or other way to measure delay and out latch...

Uwe Bonnes
Chief
January 22, 2022

10 us to 10 ms is 1000 samples. Set up a timer to sample the GPIO to DMA at 100 khz. Output the sample N ticks delayed again via DMA.

S.Ma
Principal
January 23, 2022

8 bit mcu way: timer running and overflows, get input channel capture interrupt, grab the timer captured timestamp, add your delay, write it on output compare channel. Max jitter will depends on timer run frequency, max delay will be timer overflow period. Once this works, explore a more hardware assisted solhtion.

Cedric Boudinet
Associate III
January 24, 2022

Hello. Thanks everybody for your answers.

I'll give it a try and give a feedback.

Bests