Question
Dear Ladies and Gentleman I'm a student of the University HSLU. At the moment I have been working on an porject in which I have to implement a controllsystem that is controlling and measuring the temperature and values in a bio reactor.
The bio reactor has bone marrow inside of it and this is being analysed for the properties of microgravitation.
I would use a NUCLEO-F303K8 microcontroller. The system must endure a maximum accelaration of 10G due to the fact that it will be used later on in a Fighter-Jet. My question being now, can the MCU work and function properly under such circumstances?