Skip to main content
taraben
Associate III
May 1, 2016
Question

CubeMx STM32F4 feature request implement critical section

  • May 1, 2016
  • 0 replies
  • 485 views
Posted on May 01, 2016 at 17:49

Hello ST team,

I like to see a critical section implementation similar to atmel avrlib ATOMIC_BLOCK implementation.

example:

ATOMIC_BLOCK(5) {

    uint8_t status get_spi_device_info();

    if(status == 0) return;

    do_some_more_spi_communication();

}

pls refer  http://www.nongnu.org/avr-libc/user-manual/group__util__atomic.html

and http://www.mikrocontroller.net/topic/312246#new

basically:

- the code should avoid blocking all interrupts

- the code must allow to use break and return

- the MCU status after the code must be the same as before the code squence

- the code should higher the baseprio based on given argument

- the code must not lower the baseprio if current cpuprio is higher than given baseprio

use cases:

- SPI device with notification signal

   main thead avoids to be interrupted by pin event handler

- I2C devices

  communication from main thread and ISR

- semaphore like operations

ST there is obviously a need for this and many people are implementing self brewed implementation.

Pls provide some proven code.

Regards, Adib.

--
    This topic has been closed for replies.