Question
CubeMX 4.13.0 bug - com.st.microxplorer.codegenerator.fctDefinition@2f970d
Posted on March 15, 2016 at 13:53
After I switch to new CubeMX version code generation is broken.
In main.c file stange function names generated instead of init functions. @@ -78,11 +78,11 @@ int main(void) SystemClock_Config(); /* Initialize all configured peripherals */ - MX_GPIO_Init(); - MX_CAN1_Init(); - MX_CAN2_Init(); - MX_IWDG_Init(); - MX_USART1_UART_Init(); + com.st.microxplorer.codegenerator.fctDefinition@2f970d(); + com.st.microxplorer.codegenerator.fctDefinition@1147aa8(); + com.st.microxplorer.codegenerator.fctDefinition@12a4992(); + com.st.microxplorer.codegenerator.fctDefinition@b16b36(); + com.st.microxplorer.codegenerator.fctDefinition@cc1652(); /* USER CODE BEGIN 2 */ @@ -97,7 +97,7 @@ int main(void)