I have been able to used FLASH_ProgramHalfWord, to write data into a const [] (only as long as it is initialised to all 0xFFs first.)
(FLASH_ProgramHalfWord((UINT32)&ARRAY[1],0xAA);) //writes AA into ARRAY[1], however my array size is large, (2048 bytes) this was located in ram, but to free memory usage we are moving it into flash. Because the array is so big it is not really convieniant to initialise all the data to 0xFFs, is there a way I can force ARRAY[] to be located at a fixed address? For example, 0x800E800, then I can erase my array (initialise it to 0xFFs) by Erasing the pages from 0x800E800, and 0x800EC00). Is this possible? Regards Dan
Yes, but it depends on your compiler, so you would need to post that information here.
If you are using GNU, then you need to reserve a section in your memory layout file (using KEEP and align), and then force your array into it using: const vu8 __attribute__((section(''.myflashsection''))) SomeArray[2048]; Or if you are lazy, and want to risk it, just use the last page of flash and hope that your compiler doesn't put anything there (and then use a cast to access it).