Skip to main content
oussama-laribi
Associate
April 26, 2013
Question

Capteur Internal Temperature sensor..!!

  • April 26, 2013
  • 4 replies
  • 930 views
Posted on April 27, 2013 at 00:26

Hi

I find problems with capateur internal temperature sensor STM32F4 Discovery, I have measured as false (-80.50...-45.00...-60.50 ).

I know if my code is wrong or the formula that calculates the temperature.

I hope there's someone there who has decided to issue ..!

I hope to find the right code or the right formula.

thank you..
    This topic has been closed for replies.

    4 replies

    raptorhal2
    Lead
    April 27, 2013
    Posted on April 27, 2013 at 19:41

    Check the F4 Standard Peripheral Library examples for guidance. If that doesn't work, post your code.

    Cheers, Hal

    oussama-laribi
    Associate
    April 27, 2013
    Posted on April 27, 2013 at 20:43

    The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6mp&d=%2Fa%2F0X0000000bvQ%2F0gf4DYlmjTOqdcsO4.FBltQnS2BUwM8laM1r4KiFARI&asPdf=false
    raptorhal2
    Lead
    April 29, 2013
    Posted on April 29, 2013 at 16:15

    Two problems:

    The minimum ADC sampling time for the temperature channel is 10 microseconds. See Section 5.3.21 in the F4 datasheet. Change the sampling to at least 110 cycles.

    After

    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

    Add

    ADC_InitStructure.ADC_ExternalTrigConv = 0;

    Cheers, Hal

    oussama-laribi
    Associate
    April 29, 2013
    Posted on April 30, 2013 at 01:03

    thank you Hal

    after handling with the equation .. it's oky here is the code ..: cheers, Lary.

    /* Includes ------------------------------------------------------------------*/
    #include ''stm32f4_discovery.h''
    #include <
    stdio.h
    >
    #include ''main.h''
    #include <
    math.h
    >
    #define ADC1_DR_ADDRESS ((uint32_t)0x4001204C)
    /*************declaration*****************/
    double Voltage = 0;
    __IO uint32_t ValADC = 0;
    double temp = 0;
    void ADC1_DMA_Config(void);
    void Delay(__IO uint32_t nCount);
    /*********************Configuration ADC&DMA**********************************************/
    void ADC1_DMA_Config(void)
    {
    ADC_InitTypeDef ADC_InitStructure;
    ADC_CommonInitTypeDef ADC_CommonInitStructure;
    DMA_InitTypeDef DMA_InitStructure;
    GPIO_InitTypeDef GPIO_InitStructure;
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2| RCC_AHB1Periph_GPIOD, ENABLE);
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
    DMA_DeInit(DMA2_Stream0);
    DMA_InitStructure.DMA_Channel = DMA_Channel_0;
    DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC1_DR_ADDRESS;
    DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ValADC;
    DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
    DMA_InitStructure.DMA_BufferSize = 1;
    DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
    DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
    DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
    DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
    DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
    DMA_InitStructure.DMA_Priority = DMA_Priority_High;
    DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
    DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
    DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
    DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
    DMA_Init(DMA2_Stream0, &DMA_InitStructure);
    DMA_Cmd(DMA2_Stream0, ENABLE);
    GPIO_DeInit(GPIOD);
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14| GPIO_Pin_15;
    GPIO_InitStructure.GPIO_Mode =GPIO_Mode_OUT ;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN ;
    GPIO_Init(GPIOD,&GPIO_InitStructure);
    ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
    ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
    ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
    ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
    ADC_CommonInit(&ADC_CommonInitStructure);
    ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
    ADC_InitStructure.ADC_ScanConvMode = DISABLE;
    ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
    ADC_InitStructure.ADC_ExternalTrigConv = 0;
    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
    ADC_InitStructure.ADC_NbrOfConversion = 1;
    ADC_Init(ADC1, &ADC_InitStructure);
    ADC_DMACmd(ADC1, ENABLE);
    ADC_RegularChannelConfig(ADC1, ADC_Channel_TempSensor, 1, ADC_SampleTime_480Cycles);
    ADC_TempSensorVrefintCmd(ENABLE);
    ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
    ADC_Cmd(ADC1, ENABLE);
    }
    /****************************Programme Principal********************************************/
    int main(void)
    {
    ADC1_DMA_Config();
    ADC_SoftwareStartConv(ADC1);
    Voltage = (ValADC *3300)/4095;
    temp = ((Voltage - 760)/2.5)+25;
    /********************************************/
    void Delay(__IO uint32_t nCount)
    {
    while(nCount--)
    {
    }
    }
    #ifdef USE_FULL_ASSERT
    void assert_failed(uint8_t* file, uint32_t line)
    {
    while (1)
    {
    }
    }
    #endif