Skip to main content
LMI2
Senior III
January 15, 2016
Question

Cannot connect to a Discovery card with ST-link/V1

  • January 15, 2016
  • 1 reply
  • 412 views
Posted on January 15, 2016 at 23:27

I have a discovery card F100RBT which is working. I see my old SW blinking LEDs. But now I cannot connect to it. It has been difficult before but now it seems impossible. I have tried with Keil IDE and ST-LINK. Reset active and not. All modes I could change. Nothing seems to work.

I would like use that board because all CPU pins are connected to pin headers, making the board easy to use.
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    January 16, 2016
    Posted on January 16, 2016 at 15:43

    Ok, and do the ST-LINK Utilities work with this board, and are you using the most current firmware, drivers, etc?

    In Keil you'd need to use the ''ST-Link (Deprecated Version)'' selection in the debugger to use a V1 device. There were two ST-Link debugger options in uV4.71, the old one might have been removed in newer releases.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..