Skip to main content
RGalvez
Associate
September 21, 2021
Question

CAN rollover between FIFOs after overflow in pooling mode

  • September 21, 2021
  • 0 replies
  • 443 views

Hi everyone!

I'm working with STM32F303. I'm configuring the CAN peripheral with HAL libraries for pooling mode operation.

I'm wondering if there is a method to check only the FIFO0 fill level and configure the peripheral to move FIFO1 messages into FIFO0 in entry order as it gets empty.

Is there any option or have to necessarily check FIFO1 fill level and following message reading too?

This topic has been closed for replies.