Skip to main content
freya17365
Associate III
September 18, 2015
Question

Blink program not working

  • September 18, 2015
  • 1 reply
  • 637 views
Posted on September 18, 2015 at 09:38

Hi to all,

I tried my first program on STM32F0 discovery board and I encountered some problems.

My intention is to make LED3 and LED4 blinking, so I create a main program with system initialization and a LED class to manage LEDs.

I set up system clock in main program and GPIOC clock in LED class.

Do I need something else?

In annex you can find my files.

Thank you

Freya

    This topic has been closed for replies.

    1 reply

    Nesrine M_O
    Associate
    September 18, 2015
    Posted on September 18, 2015 at 11:09

    Hi Freya,

    I'd highly recommend you to start from GPIO example under STM32Cube F0 package it describes how to configure and use GPIOs through the STM32F0xx HAL API:

    STM32Cube_FW_F0_V1.4.0\Projects\STM32F072BDiscovery\Examples\GPIO\GPIO_IOToggle

    The Cube F0 package is available on ST web site under this 

    http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF260612?s_searchtype=partnumber

    .

    -Syrine –