Skip to main content
janvi
Associate III
December 14, 2009
Question

BGA64 Availability

  • December 14, 2009
  • 3 replies
  • 848 views
Posted on December 14, 2009 at 10:36

BGA64 Availability

    This topic has been closed for replies.

    3 replies

    janvi
    janviAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:33

    We have a design with very small production quantities (

    The request at our STM representative resulted in F103R8H6 offer with a minimum order quantity of 3840 pieces and 12-16 weeks delivery time! Therefore I assume, the BGA64 never existed? If not, who is using a BGA64 and what is exact model ?

    gahelton12
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:33

    If you didn't like the LTC1661 because of setting time (30uS), then you are going to be real disappointed with the MAX5533 (660uS). :-[

    Of course, the DAC in the micro has a setting time of 3-4uS. But package size and availability seems to be a major problem.

    Here is another possibility for your DAC (Analog Devices AD5623RBCPZ). This is a Dual, 12 bit, serial DAC, Internal Reference, voltage output, 3-4.5uS setting time, small package.

    http://www.analog.com/static/imported-files/Data_Sheets/AD5623R_5643R_5663R.pdf

    Good Luck.

    picguy
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:33

    A quick look at ST’s BGA100 & 144 shows 10mm on a side for both. Therefore you have an extra millimeter on each edge. Not the best idea. Check the size of the Luminary Micro (now TI) BGA108. If it’s 9x12 and not square the 9 side might work for you. Good luck.