Skip to main content
EEtxe.1
Associate
April 8, 2021
Question

Are the 6 fast channels on an STM32h742 ADC preconfigured by default as fast or I need to configure them as fast?

  • April 8, 2021
  • 0 replies
  • 429 views

I have the package LQFP100, so the Application Note specifies that there are 3 fast channels, but the Reference Manual says that the first 6 input channels are fast channels. How is this? If I have to configure them as fast how can I do it or where can I have a look at how is it done?

This topic has been closed for replies.